Solution
Today, Rowa uses the igus product range for energy and signal supply systems as well as cables.
Even though the
chainflex cables were explicitly developed for very high stresses and intensive movements, the systems represented a special requirement profile. The frequent bending beyond a bending angle of 180 degrees and the simultaneous use of a very small radius puts a lot of stress on the cables. In order to find the optimum solution, Rowa provided the igus team with two gripper systems. Endurance tests were run in the igus laboratory and the electrical specifications of the cables were tested - with the result that in some cases different core cross sections were chosen. The focus was clearly placed on the service life so that the systems can run maintenance-free.
Specifically, chainflex
cables of the CF10 type are used as energy and control cables as well as
cables from the CF11 series as data cables. In all series, according to the tests, the conductors have an extremely bending-resistant design and construction, the special stranding ensures a lasting flexibility in multiple dimensions without core ruptures and with minimum wear. In some applications, where the cables have extremely small radii, a
control cable of the CF99 series with an alloy conductor is used, because even smaller radii are now possible.
For the energy chain, which is subjected to the same stresses as the cables, the radius of the chain had to be individually adapted due to the installation space. Here, the igus designers have done detailed work to achieve maximum availability. The
E2 series energy chains are used here in enclosed and open design on the gripper and the
2500 series for the longitudinal travel of the complete gripper system along the racks.